Use the Enable User Account dialog box
Use the
Enable User Account
dialog box to enable a user account to log in the system at runtime.To enable a user account at runtime
- Press theEnable Userbutton to open theEnable User Accountdialog box.
- PressSelect Userto open theFactoryTalk User Selectiondialog box.
- In theSelect Userfield, press theUporDownkey to select a user account.
- Press theSelectbutton, orEnter
on the external keyboard to select the user account. - Press theEnablebutton, orEnter
on the external keyboard to enable the selected user account.
The operation status shows in the
Result
box.
TIP:
You cannot use the
Enable User
button to enable a Windows-linked user. Only a Windows Domain administrator can enable a Windows-linked user from a domain computer.Provide Feedback