Add a Windows-linked user or Windows-linked user group
You may need to add a Windows-linked user or Windows-linked user group to your system.
To add a Windows-linked user or Windows-linked user group
- PressTypeto selectWindows-linked UserorWindows-linked User Group.TIP:When adding a Windows-linked user or a Windows-linked user group, the system will verify whether the user or group exists in the Windows User Accounts. If the user or group does not exist in the Windows User Accounts, it cannot be added.
- In theNamebox, type the user or group name. The name is not case sensitive.TIP:OnPanelView Plus 6andPanelView Plus 7terminals, there is a five-minute threshold when adding a Windows-linked user or a Windows-linked user group.
- When you add a Windows-linked user or a Windows-linked user group for the first time, a window prompts you to enter an authorized user name and password.
- Within five minutes after a Windows-linked user or a Windows-linked user group is successfully added, you can add another Windows-linked user, or Windows-linked user group without entering an authorized user name and password.
- Beyond five minutes after a Windows-linked user or a Windows-linked user group is successfully added, a window will prompt you to enter an authorized user name and password again before you can add another Windows-linked user, or Windows-linked user group.
Provide Feedback