Add a FactoryTalk Security user

You may need to add a
FactoryTalk Security
user to your system.
To add a
FactoryTalk Security
user
  1. Press
    Type
    to select
    FactoryTalk Security User
    .
  2. In the
    Name
    box, type the user name. The name is not case sensitive.
  3. In the
    Password
    box, type the user password. The password is case sensitive.
  4. In the
    Confirm Password
    box, type the user password again.
  5. Press the
    Advanced
    button to set the following options if needed, and click
    OK
    . The advanced settings are set to
    No
    by default.
    • User must change password at next logon
    • User cannot change password
    • Password never expires
    • Account is disabled
      TIP:
      For more information on runtime security settings, refer to "Work with the Runtime Security editor" in
      FactoryTalk View ME
      User's Guide
      .
      For more information on account policy settings, refer to "Setting up security policies" in
      FactoryTalk
      Help.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal