Runtime messages to Diagnostics for the Logout button
At runtime, the application logs information messages about the
Logout
button to diagnostics under these circumstances:Log out
- When the user logs out, the application sends a message.
- When the user logs out, the application logs a message about the System\User Account ID (for the default user).
Provide Feedback