Set up connections for a Login button
Use the
Connections
tab of the Login Button Properties
dialog box to set up a tag or expression for the button.To set up tags and expressions for the Login button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to theDomain Name.TIP:TheDomain Namemust be a string type.
Provide Feedback