Problems with logging in
At runtime, the operator uses the
Login
dialog box to log in to the system. If login is successful, the previous user is logged out and the operator is logged in.Login is unsuccessful under these circumstances:
Graphic display change
- If the graphic display changes remotely before the operator has pressed theEnterbutton in theLogindialog box, the dialog box closes and the user is not logged in. If the string pop-up keyboard is open when the display change occurs, both the keyboard and the dialog box close.
Unknown user or password
- If the user name or password does not match the settings in theRuntime Securityeditor, the user is not logged in and a diagnostics message is logged.
Provide Feedback