Runtime messages to Diagnostics for the Login button
At runtime, the application logs information and error messages about the
Login
button to diagnostics under these circumstances:Log in
- If login is successful, the application logs a message.
- If login is successful, the application logs a message about the System\User Account ID.
Unknown user or password
- If the user name or password dose not match the settings in theRuntime Securityeditor, the user is not logged in and the application logs an error.
Provide Feedback