Buttons and keys
- DomainPress this button to open the string pop-up keyboard. Use the keyboard to type the domain name, and then pressEnteron the keyboard.
- User NamePress this button to open the string pop-up keyboard. Use the keyboard to type the user name, and then pressEnteron the keyboard.
- PasswordPress this button to open the string pop-up keyboard. Use the keyboard to type the user password, and then pressEnteron the keyboard.
- LoginPress this button to finish logging in.
- CancelPress this button to close the dialog box without logging in.
- DeletePress this key on an external keyboard to clear the box that the cursor is in.
- BackspacePress this key
on an external keyboard or keypad to delete the character in front of the cursor. Hold the button down to delete multiple characters. - Left arrowPress this key on an external keyboard to move the cursor to the left.
- Right arrowPress this key on an external keyboard to move the cursor to the right.
Provide Feedback