Use the Disable User Account dialog box
Use the
Disable User Account
dialog box to disable a user account at runtime.
TIP:
When a user is disabled, the user cannot log in the system.
To disable a user account at runtime
- Press theDisable Userbutton to open theDisable User Accountdialog box.
- PressSelect Userto open theFactoryTalk User Selectiondialog box.
- In theSelect Userfield, press theUporDownkey to select a user account.
- Press theSelectbutton orEnter
on the external keyboard to select the user account. - Press theDisablebutton orEnter
on the external keyboard to disable the selected user account.
The operation status shows in the
Result
box.
TIP:
You cannot use the
Disable User Account
button to disable a Windows-linked user. Only a Windows Domain administrator can disable a Windows-linked user from a domain computer.Provide Feedback