Specify the graphic display and system-wide alarm options

To specify the graphic display and system-wide alarm options
  1. On the
    Advanced
    tab of the
    Alarm Setup
    editor, in the
    Current alarms
    box, select the graphic display used to show alarm messages.
  2. Click the
    Browse
    button to select from a list of all the graphic displays in the project.
    The specified display opens when an alarm occurs if you select the
    Display
    option for the alarm message on the Messages tab.
  3. Specify the system-wide alarm settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal