Set up on-board audit trail

Use the
Audit Trail Setup
editor to set up on-board audit trail at runtime.
TIP:
Select the
Audit trail
check box in the
Startup
editor to apply the audit trail settings.
The audit log file is automatically saved in:
  • (PC and
    MobileView
    )
    \Users\Public Documents\RSView Enterprise\ME\Logs\<ApplicationName>\M_AuditTrails\
  • (
    PanelView Plus 7
    and
    PanelView Plus 6
    )
    \Windows\Logs\<ApplicationName>\M_AuditTrails\
To set up audit trail
  1. From the
    Explore
    tree, double-click
    Audit Trail Setup
    to open the
    Audit Trail Setup
    editor.
  2. Specify the
    Maximum number of audit messages
    for the log file.
  3. (Optional) Specify these values and assign tags:
    • Capacity high warning (%)
    • Capacity high-high warning (%)
  4. (Optional) Specify a tag to
    Capacity overrun.
  5. (Optional) Specify a tag or expression to
    Remote clear audit history
    .
  6. Click
    OK
    to save the options and close the editor.
Select the
Audit trail
check box in the
Startup
editor to turn on audit trail.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal