Set up general properties for a diagnostics list object
Use the
General
tab of the Diagnostics List Properties
dialog box to set up general properties for the object.To set up general options for the diagnostics list object
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
Provide Feedback