The Component Browser

The
Component Browser
allows you to select what display, macro, image, parameter, or message file will be called when a button or display object is activated at runtime.
To specify a component
  1. Open the object’s property panel or
    Properties
    dialog box.
  2. Click the property (Display, MessageFile, ParameterFile, for example) that needs to be defined. A
    Browse
    button (...) appears at the right.
  3. Click the
    Browse
    button. The
    Component Browser
    opens with a list of the components of that type available in the project.
  4. Select the component (parameter or message file, display, macro, or image) to be called when the object is activated at runtime, that is, when the button is pressed or the display object is clicked.
  5. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal