Assign connections to an object

The
Connections
tab of the
Property Panel
shows all the object’s connections that can have a tag or expression.
If more than one object is selected on the display, nothing shows on the
Connections
tab.
If a third-party ActiveX control is selected, the
Connections
tab shows all the ActiveX control's properties that can have a tag or expression assigned.
TIP:
To get help for the selected control in the
Property Panel
, click the
?
button.
To assign connections to an object
  1. On the
    Connections
    tab, click a connection's row to select it.
  2. In the
    Tag/Expression
    column, specify a tag name, or specify an expression if the connection accepts expressions and you want to assign one.
    TIP:
    To select a tag from the tag database, click the
    Browser
    button (...) in the
    Tags
    column.
    To open the
    Expression
    editor, click the
    Browser
    button (...) in the
    Exprn
    column.
  3. Press
    Enter
    or click another cell in the grid to save the tag or expression assignment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal