XYPlotAxisPen
Specify which pen serves as the X-Axis in an X-Y plot.
A trend chart can plot values against time or against a selected pen. This property takes effect only when the ChartStyle
property is set to XYplotStyle
. If the ChartStyle
property is not set to XYplotStyle
, the value is always zero.Provide Feedback