WriteOnEnter

Specifies whether to write to the data source when the operator presses an
Enter
key button object or the
Enter
key on an external keyboard/keypad while the Control List Selector is the selected object on the display.
If you select
False
, the application writes the state value to the data source as soon as a new state is highlighted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal