WordWrap, CaptionWordWrap or St_CaptionWordWrap
Specifies whether the text continues onto the next line at the beginning of a new word.
If WordWrap is False, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object or column and the font size.
Provide Feedback