WidthTriggerValue
Type a value between 1 and 255 for the width, in characters, of the
Trigger Value
column that will be printed when the Print Alarm History
or Print Alarm Status
button is pressed. The default value is 11.Provide Feedback