Visible States
A write connection for the piloted control list selector. Assign an array tag or an expression to this connection. When the list scrolls, the values associated with the states that are visible on the list will be written to the data source. The number of elements in the array tag must match the number of visible states.
Provide Feedback