Visible or (GroupVisible)
Specifies whether to make the object or group visible.
If this is False, the object is invisible at runtime. (It is visible in the development system.)
If you are using visibility animation, the visibility animation setting overrides this option.
TIP:
If an object is not visible at runtime, it is not functional. Clicks or touches on an invisible object pass through the object to whatever is behind it.
Provide Feedback