Value

A write only connection. Assign a tag or expression that can support up to 82 characters (bytes). When the operator presses the
Enter
key, the application writes the alphanumeric string to the tag’s data source
.
If you do not assign the Value connection, at runtime when the operator presses the button, the string pop-up does not open.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal