Value
A read-write connection. Assign a tag to this connection. When the operator selects a state, the application writes the value corresponding to the selected state to the tag’s data source. The application also monitors this connection and if the value changes, highlights the new state in the list.
TIP:
If the WriteOnEnter property is True, the application doesn’t write to the Value connection until the operator selects a state and presses
Enter
.If the WriteOnEnter property is False, the Enter and Enter Handshake connections are ignored.
Provide Feedback