Value

A read-write connection. The application keeps a copy of the Value connection on the computer. When the operator presses the
Ramp
button, the application adds or subtracts the RampValue amount from the local Value connection value and writes the result to the Value connection tag’s data source.
TIP:
If the RampValue property is a floating point value and the Value connection is an integer tag, the application rounds the value before writing it to the connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal