Choose whether the object's Ramp value will use a tag or expression value (True), or a constant value (False), at runtime. If a constant value is used, the RampValue property must be specified. If a tag or expression value is used, the Ramp connection must be assigned.