UseEchoMessage
Specifies whether to use an echo message.
If this is
True
, the echo message function is used and the triggered message will be written to the string tag assigned for the Echo Message connection.If this is
False
, the echo message function will not be used.Provide Feedback