TimeFormat

Specify in what time format the trend shows. This setting affects every time display in the trend object.
The available options are:
  • 12-hour (AM/PM)
  • 24-hour
  • Use system time setting
If system time format is selected, the format specified in the
Windows Control Panel
's
Regional Options
is used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal