Status Reset connection

A write connection. Assign a digital tag to this connection to notify the data source that the alarm status has been reset, that is, the accumulated time for all alarms has been reset to 00:00:00, and the alarm quantity for all alarms has been reset to 0.
When the application starts, this connection has a value of zero. If the operator presses a
Reset Alarm Status
or
Clear Alarm History
button, the connection is set and held for as long as the button is pressed, or for the notification hold time, whichever is longer.
If the Remote Status Reset connection causes the reset, the Status Reset connection is set and held for the notification hold time. The connection is then reset to zero.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal