State

Specifies the state whose properties are displayed in the St_... properties. Select a different number to edit a different state, or use the States toolbar to select a different state.
The released state is State 0. The pressed state is State 1.
When the button’s connection tag value equals the value for this button, the button is in State 1. If the connection tag is any other value, the button is in State 0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal