State

Specifies the state whose properties are displayed in the St_... properties. Select a different number to edit a different state, or use the States toolbar to select a different state.
The released state is State 0. The pressed state is State 1.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal