St_Access

Specifies who has access to the piloted control list selector's selected state. The options are:
  • Operator and Remote
    - both a user and a remote controller can select the state
  • Operator
    - only a user can select the state
  • Remote
    - only a controller can select the state
  • None
    - the state cannot be selected
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal