Shape

Specifies the shape of the button. The available options are:
  • Rectangle
  • Circle
  • Ellipse
If the button's shape is a circle or ellipse, the button’s touch area remains a rectangle, and the width, height, and other properties apply to the button's bounding box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal