Scroll

Specifies whether the chart continually updates with new data during runtime.
If the
Scroll
property is set to
False
, the chart fills with new data up to the limit specified in the
BufferSize
property. Beyond that point, the chart does not update with new data until the operator manually toggles the scroll mode using the
Pause Pen
button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal