Remote Status Reset connection

A read connection. Assign a tag or expression to this connection. When this connection changes to a new non-zero value, the alarm status is reset. All accumulated alarm times are reset to 00:00:00, and all alarm quantities are reset to 0. If an alarm is still active when the alarm status is reset, its accumulated time will continue from 00:00:00 and its alarm quantity will increase from 0 to 1.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal