Remote Access
A read-only connection. Assign a tag to this connection. If this connection is a non-zero value, the piloted control list selector is controlled remotely. If the connection is set to zero, the operator controls the object.
Provide Feedback