ParameterList or St_ParameterList

Specifies the parameter list to run when the button is pressed or when the operator highlights this state and presses
Enter
. Click the
Browse
button (...) to open the
Tag Browser
and add tags to the list. Each new tag is separated from the previous tag by a comma.
A parameter list assigns tags to tag placeholders in the display when the display opens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal