ParameterFile
Specifies the parameter file to run when the button is pressed. Click the
Browse
button (...) to open the file selector. The selector's list contains all of the parameter files in the project.A parameter file assigns tags to tag placeholders in the display when the display opens.
Provide Feedback