MessageFile

Specifies the message file to use with the local message display. Click the
Browse
button (...) to open the
Local Message Selector
. The selector's list contains all of the local message files in the project.
If a variable message file is used, this is disabled and the application uses the string tag or expression specified for the
Message File
connection as the message file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal