LinkConnections

Specifies whether the reference object will use the connections assigned to the base object.
If the property is True, the object's connections will be read-only, and cannot be edited by the user.
If the property is False, the reference object can have other connections assigned. These connections will not affect the base object, and any changes to the base object's connections will not be picked up by the reference object.
Only reference objects that support a connection will have this property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal