LineStyle
Specifies the line style. If you select a style other than Solid, the LineWidth property must be 1 pixel.
For the gauge object, this property applies to the dial outline and tick marks.
TIP:
The dash-dash-dot and dash-dot-dot formats display as dot format in
PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, or PanelView Plus CE
at runtime.Provide Feedback