Indicator

A read-only connection.
You can assign a tag or an expression to this connection. The application reads the value of the connection at the data source, and updates the object’s display to reflect the state corresponding to the value.
If you assign an expression, the application calculates the value of the expression and updates the object’s display to reflect the state corresponding to the value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal