InactiveUnacknowledged

A read-only connection. Assign a tag or an expression to this connection. At runtime, when the tag or expression value is- non-zero, the
Alarm
list shows alarms that are no longer active and have not yet been acknowledged.
If you assign an expression to this connection, the application calculates the value of the expression and uses the result to determine whether to show inactive unacknowledged alarms.
When this connection is assigned, it overrides the DisplayInactiveUnackedAlarms property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal