ImageBackStyle or St_ImageBackStyle
This property applies to both monochrome and color images. Use it to set the background style to Solid or Transparent.
For monochrome images, if the ImageBackStyle is set to Transparent, the background will be transparent.
For color images that are not PNG with Alpha channel, if the ImageBackStyle is set to Transparent, any parts of the image that are black will be transparent.
Provide Feedback