Image scaled
If selected, the image scales to the size of the button.
If not selected:
- When the image is larger than the button, the image is clipped to fit into the button.
- When the image is smaller than the button, theAlignmentoption determines the image’s position on the button.
Provide Feedback