Image back style
Specifies whether the image’s background is visible or hidden. If the background is visible (Solid), the image’s background color is the Image back color. If the background is hidden (Transparent), anything behind the image will show through the background.
Provide Feedback