Format
Specifies the time and date format to show. For the alarm list object, this format is used for the alarm time and acknowledge time.
The options reflect the settings in your development computer’s operating system. If the operating system settings are different on your development and runtime systems, the runtime settings are used at runtime.
Provide Feedback