FixedPosition
Specifies the kind of output to use with the Fixed position decimal point:
- Stripped valueThe decimal point will be stripped out of the shown value and the resulting integer will be written to the Value connection.
- Displayed valueThe shown value will be written to the Value connection without any changes.
Provide Feedback