EnterKeyHoldTime
Specifies the time the Enter connection will be set to 1. This time setting applies only if the Enter connection is assigned and the Enter Handshake connection is not assigned on the
Connections
tab.Provide Feedback