EnterKeyHandshakeTime

Specifies the maximum time the Enter connection will be set to 1. This time setting applies only if the Enter and Enter Handshake connections are both assigned on the
Connections
tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal