EnterKeyControlDelay

Specifies the length of the delay between the time the operator presses the
Enter
button and the time the application sets the Enter connection to 1. Assign the Enter connection on the
Connections
tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal