Deadband

Specify a percentage, from 0% to 100% of the actual value, by which a value must change before the chart shows the next value.
This property applies only when the
ChartMode
property is set to
On Change
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal